Is there an error in the code for bus voltage compensation?
My configuration:
- [VERSION]: MCSDK 6.3.2
- [TOOL]: MC Workbench, ST MOTOR Pilot
- I am using the HSO on a custom board with an STSPIN32G4 at 15 kHz.

The basic algorithm here should be the reciprocal of the bus voltage, using LPF filtering for result. So the code should be modified as follows. Please help me confirm whether my understanding is incorrect or if there is indeed an error here?