Issue with Workbench 6.4 and Motor Profiler
- October 21, 2025
- 1 reply
- 276 views
I've gotten myself into an odd bug or something. I had been using the Motor Profiler successfully from the Workbench for a month or so and I had to stop for a while and work on other items. I may have played around the graphing/plotting stuff in Motor Profiler the last thing I did. Not totally sure.
When I went through the normal connection process to run Motor Profiler today I got a weird pop up that only stays on for 2 seconds and then disappears. I'm not sure if I've ever seen this screen before. It could be a GUI. It could be settings for a plot, but it is not the Motor Profiler GUI that I expected. I captured the 2-second pop up from a video in the attached image.
Does anyone know if this is a bug or corrupted files or settings. How do I reset Workbench to get it to just open the profiler GUI again?
Thanks for any assistance you can provide.