MC workbench showing the message Code generation completed with error
Hi I have added the required details in the MC workbench and clicked on "Generate the project" After that, the below window pops up.

in that under Firmware Package Version it is providing the three option to select
1. STM32 FW V1.11.5
2.STM32 FW V1.11.4 (Recommended , not installed)
3. Latest
from that I have selected the STM32 FWV1.11.5 option and clicked on the <Generate> button , but it completing the project generation with error.
I need you inputs on the below points
1. why project is generating with error , how I can resolve this error
2. the second option STM32 FW V1.11.4 , where I will get this and what is the process to added this in the project , so that it will detect in the dropdown list in MC workbench.
In advance thankyou for your support.