Skip to main content
TLi.5
Associate II
November 23, 2023
Question

MCSDK 6.2 Motor pilot cann't choose Control Board and Power Board

  • November 23, 2023
  • 3 replies
  • 1273 views

Dear STer

        I use MCSDK 6.2 ,I want  use  UNCLEO-G431RB + X-NUCLEO-IHM07M1   profiler motor model ,but open “motor profiler” ,Control Board and Power Board is blank。

Picture1.png

    This topic has been closed for replies.

    3 replies

    SRedd.5
    Senior III
    November 24, 2023

    According to my understanding first you have to connect the board using UART.

    TLi.5
    TLi.5Author
    Associate II
    November 24, 2023

    Thank you for your reply!I have connected the development board through uart. You can also see from the picture that the baud rate is 1843200bps.I changed to another PC and the problem did not change.

     

    SRedd.5
    Senior III
    November 24, 2023
    cedric H
    Technical Moderator
    November 24, 2023

    Hello @TLi.5 

    The new strategy is to allow you to generate your own profiler project with the workbench.

    Doing so, you will be able to select the combination you want, and to tune the PWM frequency according to your motor. 

    To do so, please read the documentation available at the highlighted location on the screenshot below.

     

    cedricH_0-1700836464870.png

    Regards

    Cedric