Skip to main content
Associate
July 30, 2024
Question

MCSDK-PKG001/STEVAL-PTOOL1V1_6S_HL fails to compile

  • July 30, 2024
  • 1 reply
  • 670 views

Hi,

MCSDK-PKG001/STEVAL-PTOOL1V1_6S_HL fails to compile with the errors below:

 

C:/Users/Ian/.st_workbench/projects/MCSDK-PKG001/STEVAL-PTOOL1V1_6S_HL/Src/mc_tasks.c: In function 'MC_RunMotorControlTasks':
C:/Users/Ian/.st_workbench/projects/MCSDK-PKG001/STEVAL-PTOOL1V1_6S_HL/Src/mc_tasks.c:221:9: warning: implicit declaration of function 'SixPwm_TurnOnLowSides'; did you mean 'PWMC_TurnOnLowSides'? [-Wimplicit-function-declaration]
221 | SixPwm_TurnOnLowSides(pwmcHandle[M1],M1_CHARGE_BOOT_CAP_DUTY_CYCLES);
| ^~~~~~~~~~~~~~~~~~~~~
| PWMC_TurnOnLowSides

C:/Tools/STM32/STM32CubeIDE_1.16.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.12.3.rel1.win32_1.0.200.202406191623/tools/bin/../lib/gcc/arm-none-eabi/12.3.1/../../../../arm-none-eabi/bin/ld.exe: ./Application/User/mc_tasks.o: in function `MC_RunMotorControlTasks':
C:/Users/Ian/.st_workbench/projects/MCSDK-PKG001/STEVAL-PTOOL1V1_6S_HL/Src/mc_tasks.c:221: undefined reference to `SixPwm_TurnOnLowSides'

    1 reply

    Fabrice LOUBEYRE
    ST Employee
    August 9, 2024

    Hi murpia, these two examples STEVAL-PTOOL1V1_6S_HL.ioc and STEVAL-PTOOL1V1_6S_SL.ioc must be generated with the followed setup (information embedded into the IOC file):

    STM32Cube FW_F0 V1.11.4

    CubeMxCube.Version=6.9.1 or above (i used 6.9.11)

    MCSDK_v6.2.0

    With this setup the two examples compile with STM32CubeIde.

    Best Regards.

    Fabrice