Skip to main content
Associate III
February 20, 2025
Solved

MCSDK5.4.8 motorcontrol reference pack not found

  • February 20, 2025
  • 5 replies
  • 1785 views

系統 : Windeows 10 22H2

應用 : MCSDK5.4.8 CubeMax6.13

目標工具鏈 : ST32CubeIDE

固件包版本 : STM32 FW v1.11.3

為什麼在從未修改的範例專案生成代碼時會收到此錯誤?

未命名.png

Best answer by GMA

Hello @walen,

Firstly, as mentioned in st community terms and conditionsthe language of the Community is English.

Refer to MC Workbench Release note documentation:

GMA_0-1740040875975.png

On "V5.4.8 / 30-Nov-2021" chapter, it is mentioned CubeMx version to be used "v6.4.0" and firmware packages versions for each STM32 series.

5 replies

GMA
GMABest answer
Technical Moderator
February 20, 2025

Hello @walen,

Firstly, as mentioned in st community terms and conditionsthe language of the Community is English.

Refer to MC Workbench Release note documentation:

GMA_0-1740040875975.png

On "V5.4.8 / 30-Nov-2021" chapter, it is mentioned CubeMx version to be used "v6.4.0" and firmware packages versions for each STM32 series.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA
walenAuthor
Associate III
February 20, 2025

Hi Dear All,

Based on the suggestions, what is the meaning and reason for the following situation?

Thank you for the response. Previously used community-specific language. Still learning...

APP: CubeMax6.4 , STM32 FW v1.8.4

20250220_175550.png20250220_175542.png

 

GMA
Technical Moderator
February 20, 2025

Hello @walen;

As the generation has gone up to the main.c file, can you continue with the generated project?

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA
walenAuthor
Associate III
February 21, 2025

Hi GMA,

Yes, the main.c is shown in the project, but as depicted, the compilation failed.now?

walen_0-1740124086035.png

 

 

walenAuthor
Associate III
February 21, 2025

Hi GMA,

Can the red PDSC file affect the project?

Because the pins generated by MAX do not include my options.

未命名_1.png未命名_2.png

I our future interactions with great interest.

Thank you
Walen

 

GMA
Technical Moderator
February 21, 2025

Hello @walen,

B13/B14/B15 are shown in gray on "Control Stage" window, so they are not used.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA
walenAuthor
Associate III
February 21, 2025

hey guys, 

Someone has asked a question regarding issue 5.4.85, but I haven't seen an answer. Could you please provide assistance?

Similar to my question 

walenAuthor
Associate III
February 24, 2025

Dear GMA,

Could the issues I mentioned be because I didn't open CubeMX before opening SDK 5.4.8? Since CubeMX 6.13 is a later version than CubeMX 6.4, are there any solutions? My company requires IT personnel for installations and uninstalls.

 

walen_0-1740383208563.png

thank you  

 walen