Skip to main content
Explorer II
January 22, 2025
Question

Motor Control Workbench, STM32CubeMX error

  • January 22, 2025
  • 1 reply
  • 1599 views

dgrugur_0-1737533616351.png

dgrugur_1-1737533666009.png

dgrugur_2-1737533855816.png

dgrugur_3-1737534578043.png

 

Hi,

When I want to generate the code, it says that the STM32CubeMX version is not supported.

Also in the STM32CubeIDE Pinout & Configuration page I don't see "X-CUBE-MCSDK" in the "Middleware and Software Packs" tab.

How can I solve this problem?

Motor Control Workbench in: C:\Program Files (x86)\STMicroelectronics\MC_SDK_6.3.2
STM32CubeMX in: C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX
(It was installed in the locations it automatically selected during installation.
 Both are installed for "all users".)
OS: Windows 10 Pro
OS language: Turkish


 

1 reply

GMA
Technical Moderator
April 11, 2025

Hello @dgrugur,

Firstly, we would like to apologize sincerely for the delay in replying to your post.
Could you check the response in this post?

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA