Motor does not start
Tools:
- MCSDK - 6.2.1
- MC Workbench 6.2.1
- STM32CubeMX - 6.10
- STM32CubeIDE - 1.14.1
- ST Motor Pilot - 1.2.5
Hardware Setup
- Nucleo-0G474RE
- STEVAL-IPM30B (My own version of the board, same circuit and layout)
- X-NUCLEO-IHM09M2
- I-PMSM motor 9 Pole Pairs, 220W, 36V
DETAIL
Unable to start the motor.
First attempt to start the motor always results in an Over Current Fault.
All three of the low side PWM signals go high at the same time
Second attempt - Motor Pilot Status - Goes from WAIT_FOR_MOTOR then START.
I only seem to be getting a PWM signal on PWM-A-H, current is drawn for about 5 seconds.
EXPECTED BEHAVIOUR
I would expect PWM to be generated for each phase 120 out of phase with each other.
Then I would expect the motor to start turning.