Motor is not spinning
Dear all,
I have a NUCLEO-F302R8 and the X-NUCLEO-IHM07M1 motor driver expansion board. I have a three phase BLDC motor with an encoder attached to it. I have profiled the motor and I am able to run the motor in the profiler. When I use the workbench software to implement a speed controller or a torque controller the motor does not spin. Attaching the encoder to an oscilloscope has shown a correct signal. When I use the torque controller, it seems that the motor is trying to keep a constant position. Nothing happens when a speed controller is active. Do you have any ideas on how solve the problem and get the motor to work?