Motor Jerks at start and multiple Speed Feedback faults
I have multiple issues while driving the vehicle with the MCSDK software running. It is custom hardware MCSDK6.4.0
Hall sensor based.
1. Every time i start the vehicle at the beginning it jerks and then picks up, the behavior is not predictable, but jerking is always there some times more, less and hall fault etc. Now i have tested again on the bench and captured the waveform of the phase currents

The first few steps before the sinusoidal phase currents is problematic, so if i count i get 3 jerks before the motor started running. Can i eliminate this? It always happens when i start. Does it have anything to do with hall placement angle. I have not run the Motor pilot as i don't have the setup for that. I can perform multiple iterations of trial and error for the placement angle if the above angle is a problem at present it is 30. And my forward movement and reverse does not have the same placement angle may be due to the motor design.
Next major problem is intermittent speed feedback fault i can't predict when it happens this mainly occurs when i am starting the vehicle and also intermittently. On the bench i have tried to produce the issue

Measured angle started deviating from the super angle and fault happens.


Both the above are the same scenario 0x20 fault

All the start and stop scenarios all in between i find jerks.

Starting jerk before starting.
I have taken several failure graphs, if you can suggest me the correct direction i can look into. My only question the behavior shall be predictable but it is not.