Solved
Motor pilot connection issue
- April 13, 2026
- 3 replies
- 192 views
Hi Team,
I am working on a custom board with STSPIN32F0601S3, after generating code using MCSDK Version 6.3.0 with cube Mx 6.10.0, I tried to connect Motor pilot just start/stop and change RPM but it did not connect, Pls confirm which steps I am missing
Below are the steps I followed but still it did not connect
1.Uploaded and RUN code (using cube ide)
2. RESET board
3. Opened workbench and selected Motor Pilot
but it leads to default App Mode (pls refer screenshot) not detecting firmware although code is in run mode and not able to use Motor pilot which was along with MCSDK Pack 6.3.0