Motor Pilot HSO Hardware Config Write Error
- November 13, 2025
- 2 replies
- 245 views
Hello,
I am having an issue writing the Hardware Config in the HSO Motor Pilot. I was able to do this with my previous set up, but recently upgraded from Windows 10 to Windows 11. Along with the OS upgrade, I also installed the latest releases for all the ST software so MC Workbench went from V6.3.2 to 6.4.1. I am wondering if this is a Win 11 issue or a MC Workbench issue, or possibly a debugger setting issue?
Components Used:
MC Workbench V6.4.1
STM32CubeMX V6.15.0
STM32CubeIDE V1.19.0
B-G473E-ZEST1S Control Board
STEVAL-LVLP01 Power Board
Process:
Generate project in MCWB (Sensorless HSO option) - if errors finish generating in CubeMX - Open in CubeIDE - Build / Flash with default debugger settings via USB to onboard USB STLINK - Connect to MotorPilot (Connects fine, can tune, edit values) - Select Hardware Config (either Read / Fill from UI / Import, all with same result) - Click "Write" then the board doesn't reconnect.
The errors I get in the connection bar either say "Port Open and try to configure the board" or "Port Open but no answer from board".
I have attached the log from one such session to this post.
I have not yet tried reverting to a previous version of any software yet. Would prefer to avoid that. Any help would be appreciated.
Thanks