Motor speed issues B-G431B-ESC1
Hi!
Trying to use a Leopard LC2830-980KV motor with the B-G431B-ESC1.
I have managed to program the device with the MC Workbench and can run the motor using the Motor Pilot software. However I can't seem to get the speed over 2100 rpm for some reason.
I can get the motor to speed up to 2100 pretty rapidly when playing with the rev-up settings, but when I request a faster speed it just stays at 2100 rpm and starts to draw more current until eventually my power supply (5A) goes into over current.
Any tips on what I can check/test?
Thanks,
Carl