Skip to main content
Associate III
August 12, 2024
Question

Need evaluation kit for STM32G473 running high voltage BLDC motor

  • August 12, 2024
  • 3 replies
  • 1015 views

Hi,

I want to evluate STM32G473 based MCU for driving BLDC motor. 

Can you suggest a development kit which has:

- STM32G47 MCU

- High Voltage motor driver circuit upto 600 V (like in EVSPIN32F0251S1)

 

    3 replies

    STTwo-32
    Technical Moderator
    August 12, 2024

    Hello @mdalal and welcome to the ST Community :smiling_face_with_smiling_eyes:.

    The only Board based on an STM32G473 is the B-G473E-ZEST1S that is a part of the motor-control development platform supporting ZeST and HSO algorithms. B-G473E-ZEST1S is a control board with the STM32G473QET6 microcontroller in the ZeST Discovery pack and works together with a Power board such as STEVAL-LVLP01, an optional adaptor board such as B-ZEST-ADAPT1, and an accessories package such as B-MOTOR-PMSMA1. The B-G473E-ZEST1S control board is connected to the power board or adaptor board through an embedded MC connector V2. B-G473E-ZEST1S can also support motor driver expansion boards X-NUCLEO-IHM08M1, X-NUCLEO-IHM09M1, and X-NUCLEO-IHM16M1 via the Morpho MC connector. 

    For more details, I've escalated your post to our online support. An FAE will contact you to provide dedicated support for your request.

    Best Regards.

    STTwo-32

    mdalalAuthor
    Associate III
    August 12, 2024

    Thanks for the reply.

    I am looking for using G series to driver high voltage BLDC motor. Please let us know if any kit can be made available so that we can start developing a prototype based on it.

    STTwo-32
    Technical Moderator
    August 12, 2024

    You will soon be contacted by one of our FAEs. He will provide you all informations you are looking for.

    Best Regards.

    STTwo-32

    Billy OWEN
    ST Employee
    August 12, 2024

    Hi @mdalal 

     

    This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

     

    Regards,

    Billy