Question
Not possible to create motor control project with FOC with custom power board
- July 22, 2024
- 1 reply
- 2812 views
I am unable to create motor control project with FOC algorithm using custom power. It generates an error:
It is not possible to create a motor control project with the FOC algorithm using the selected hardware. No proper path for motor control signals was found for the following mandatory features:
- Current Sensing
For more details, please, look at the following log file in your home directory: .st_workbench/connectAlgo.log
Although I've added current sensing and the report generated is fine.
Not sure what I'm doing wrong. I've also attached the log file.