Overcoming problems with center-aligned PWM using burst-mode DMA
As an exercise, I have written a 2-phase induction motor control program using high-level program elements (HAL). I used a Nucleo-G071, though I'm sure nearly any STM32 family device will work. Since 2-phase algorithms are not common cookbook items, I started from scratch. The desired end state is the use of center-aligned PWM using burst-mode DMA and a 3-wire interface. I encountered problems with asymmetry in the pulse positions of the 3 outputs. After much coding and experimentation with logic analyzers and oscilloscopes, I came up with a method that yields a clean uniform output. I used VS Code and GitHub Copilot during the development. After finishing, I asked GitHub Copilot to summarize the problems and solutions. Perhaps this may be useful to those who are undertaking similar work. I am attaching that summary here:
# Solving Center-Aligned PWM Asymmetry in STM32 DMA Burst Mode Applications
**A Novel Split-and-Phase-Shift Algorithm for Motor Control**
*Paper developed with assistance from GitHub Copilot*
## Abstract
This paper presents a practical solution to center-aligned PWM asymmetry issues encountered when using STM32 timer DMA burst mode for motor control applications. We describe a novel "split-and-phase-shift" algorithm that eliminates concatenation artifacts in lookup table-based PWM generation while maintaining sinusoidal motor drive characteristics. The solution was implemented and verified on STM32G071 hardware using a 384-element lookup table for 2-phase motor control.
## 1. Introduction
STM32 microcontrollers offer powerful timer peripherals with DMA burst mode capabilities, enabling efficient PWM generation for motor control applications. However, when implementing lookup table-based sinusoidal PWM using center-aligned mode, developers may encounter timing asymmetries that manifest as concatenation artifacts in the PWM output. This paper documents a systematic approach to identifying and resolving these issues.
### 1.1 Problem Statement
Center-aligned PWM mode is essential for motor control applications requiring symmetric pulse generation. However, when DMA updates occur at arbitrary points in the PWM cycle, the resulting output may exhibit:
- Visible concatenation between different duty cycle values
- Asymmetric pulse timing despite center-aligned configuration
- Glitches during transitions between lookup table entries
These issues are particularly problematic in motor control where smooth sinusoidal drive signals are critical for proper operation.
## 2. Technical Background
### 2.1 STM32 Timer DMA Burst Mode
The STM32 timer DMA burst mode allows efficient updating of multiple timer registers (CCR1, CCR2, CCR3) simultaneously. Configuration involves:
```c
// Configure DMA burst base address and length
TIM1->DCR = (TIM_DMABASE_CCR1 << TIM_DCR_DBA_Pos) | ((3-1) << TIM_DCR_DBL_Pos);
// Start DMA transfer from lookup table to timer registers
HAL_DMA_Start_IT(&hdma_tim1_up, (uint32_t)lookup_table, (uint32_t)&TIM1->DMAR, array_size);
```
### 2.2 Center-Aligned Mode Timing
In center-aligned mode, the timer counts up to the period value, then counts down to zero. PWM outputs change state when the counter matches the compare values, creating symmetric pulses around the center point. The critical insight is that DMA updates must be synchronized with the PWM cycle to avoid timing conflicts.
### 2.3 Original Implementation Issues
Initial implementation used a 192-element lookup table with triplets representing {CCR1, CCR2, CCR3} values:
```c
const uint16_t original_table[192] = {
666, 0, 666, // Triplet 1
812, 0, 663, // Triplet 2
// ... more triplets
};
```
Logic analyzer testing revealed concatenation artifacts when transitioning between triplets, particularly visible during alternating duty cycle patterns.
## 3. The Split-and-Phase-Shift Solution
### 3.1 Root Cause Analysis
The concatenation problem stems from DMA timing relative to the PWM cycle. When DMA updates occur during PWM transitions, the resulting output exhibits timing artifacts. The solution requires ensuring DMA updates align properly with the center-aligned PWM timing.
### 3.2 Algorithm Development
Our solution employs a three-step process:
1. **Split each triplet in half**: Each original triplet {A, B, C} becomes two half-triplets {A/2, B/2, C/2}
2. **Handle odd numbers**: For odd values, the larger half comes first
3. **Phase offset**: Move the first half-triplet to the end of the array
### 3.3 Implementation Details
```c
// Original 64-triplet table becomes 384-element table (64 * 6 elements)
const uint16_t SRC_Buf_2Phase[384] = {
// Starting with second half of first triplet for phase alignment
333, 0, 333,
// Each original triplet split: {812, 0, 663} becomes:
406, 0, 332, 406, 0, 331, // First half, second half
// Continue for all 64 original triplets...
// ...
// Phase offset: First half of original first triplet at the end
333, 0, 333
};
```
### 3.4 Mathematical Foundation
For any original triplet {A, B, C}:
- First half: {⌈A/2⌉, ⌈B/2⌉, ⌈C/2⌉}
- Second half: {⌊A/2⌋, ⌊B/2⌋, ⌊C/2⌋}
The phase offset ensures DMA updates occur at optimal points in the PWM cycle, eliminating concatenation artifacts.
## 4. Implementation and Results
### 4.1 Hardware Configuration
- **Microcontroller**: STM32G071RB (NUCLEO-G071RB)
- **Timer**: TIM1 in center-aligned mode 1
- **DMA**: Burst mode updating CCR1, CCR2, CCR3
- **PWM Frequency**: 3.84 kHz (60Hz × 64 pulses)
- **Motor Control**: 2-phase with 90° phase relationship
### 4.2 Verification Method
Testing used both logic analyzer and oscilloscope to verify:
- PWM frequency accuracy
- Center-aligned symmetry
- Elimination of concatenation artifacts
- Proper 90° phase relationship between outputs
### 4.3 Results
The split-and-phase-shift algorithm successfully:
- Eliminated all visible concatenation artifacts
- Maintained proper center-aligned symmetric pulses
- Preserved sinusoidal characteristics for motor control
- Achieved smooth transitions between all lookup table entries
## 5. Application to Motor Control
### 5.1 2-Phase Motor Drive
The implementation provides differential outputs:
- **Phase A**: CH1 - CH3 (0° reference)
- **Phase B**: CH2 - CH3 (90° phase shift)
This configuration enables efficient 2-phase motor control with minimal hardware complexity.
### 5.2 Performance Benefits
- **CPU Efficiency**: DMA handles all PWM updates autonomously
- **Timing Precision**: Hardware-based updates ensure consistent timing
- **Scalability**: Algorithm extends to larger lookup tables
- **Flexibility**: Maintains compatibility with STM32CubeMX code generation
## 6. Comparison with Existing Solutions
### 6.1 STM32 Motor Control SDK
The X-CUBE-MCSDK uses Space Vector PWM (SVPWM) with real-time calculation, avoiding lookup table timing issues entirely. However, this approach requires higher CPU overhead and more complex implementation.
### 6.2 Advantages of Our Approach
- Lower CPU overhead than real-time calculation
- Deterministic timing characteristics
- Simple implementation suitable for cost-sensitive applications
- Compatible with standard STM32 HAL libraries
## 7. Conclusions and Future Work
The split-and-phase-shift algorithm provides a practical solution to center-aligned PWM asymmetry in DMA burst mode applications. This technique enables efficient motor control implementation while maintaining the timing precision required for professional motor drive applications.
### 7.1 Key Contributions
1. Identification of center-aligned PWM timing issues in DMA applications
2. Development of split-and-phase-shift algorithm for phase alignment
3. Practical implementation for 2-phase motor control
4. Verification methodology using standard test equipment
### 7.2 Future Applications
The algorithm can be extended to:
- 3-phase motor control systems
- Higher resolution lookup tables
- Other STM32 timer configurations
- Variable frequency drive applications
## 8. Implementation Guidelines
### 8.1 Step-by-Step Implementation
1. **Generate base lookup table**: Create sinusoidal values for desired motor control
2. **Apply split algorithm**: Convert each triplet to two half-triplets
3. **Implement phase offset**: Move first half-triplet to array end
4. **Configure DMA burst mode**: Set up timer for 3-register burst transfer
5. **Verify with test equipment**: Confirm elimination of concatenation artifacts
### 8.2 Design Considerations
- Array size doubles from original implementation
- Memory usage increases but remains reasonable for most applications
- Algorithm preserves original sinusoidal characteristics
- Compatible with existing STM32 development tools
## Acknowledgments
This work was developed with assistance from GitHub Copilot, demonstrating the potential for AI-assisted embedded systems development. The solution was implemented and verified on STM32G071 hardware using standard development tools.
## References
- STM32G0xx Reference Manual (RM0444)
- X-CUBE-MCSDK Motor Control Software Development Kit
- STM32 Timer Cookbook Application Notes
- Center-Aligned PWM Mode Documentation
---