Overvoltage error BLDC motor
Hello,
I'm using the EVSPIN32G4 Eva board and MCSDK 6.2
The motor is a low-induction 1pole pair 45000rpm 24Vdc Power 160W
The motor should work with a current up to 6A
In the motor profiler I cannot enter a value greater than 4A otherwise I have Overvoltage error during profiling
Due to this limitation I cannot use the blower up to its maximum
do you have any clues?
The overvoltage error occurs also in the motor pilot.
when the motor is running, a sudden variation of the speed cause the Overvoltage error
Last but not the least, the motor is spinning but it becomes hot very quickly
Thank you for your help
Emanuele

[VERSION]: Version of MCSDK 6.2.0
[TOOL]: MC PROFILER, MC PILOT + EVSPIN32G4 Evaluation board
[DETAILS]:Overvoltage error
[EXPECTED BEHAVIOR]: to control the speed of a BLDC blower
[HOW TO REPRODUCE]:set motor nominal current, apply a moderate speed variation