Skip to main content
Associate
October 23, 2025
Question

P-NUCLEO-IHM001 Motor Kit Usage

  • October 23, 2025
  • 1 reply
  • 247 views

I am currently seeking to implement motor rotation control to any desired angle using the P-NUCLEO-IHM001 motor kit. Is this feasible? If so, how should I proceed? Are there any relevant tutorials or documentation available? Thank you.

*This post has been translated from Chinese to comply with the ST Community guidelines.

1 reply

GMA
Technical Moderator
October 23, 2025

Hello @Lzj111111,

The language of the Community is English as mentioned here.

For motor position control, you need a motor with a quadrature encoder sensor. Refer to Position Control Application note for more details.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA
Lzj111111Author
Associate
October 27, 2025

I have consulted the position control application notes and proceeded with configuration according to the documentation. However, regarding Figures 10 and 12 in the documentation, where exactly should I make the configurations as illustrated? Thank you.

 

*This post has been translated from Chinese to comply with the ST Community guidelines.

 
 
GMA
Technical Moderator
October 28, 2025

Hello @Lzj111111,

The mentioned application note corresponds to MCSDK5.x version; however, the API usage and PID tuning chapters remain valid.
For the MCSDK6.x version, refer to the Position Control link in the User Manual documentation available through Workbench tool > About > Documentations > Documentation, User Manual tab.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA