Question
Problem with Motor profiler
[VERSION]: MCSDK 6.2.0
[TOOL]: Motor PROFILER v1.2.4
EVALSTDRIVE101 + NUCLEO-F746ZG
[DETAILS]:
I have a sensorless project which work perfectly when the motor profiler option is disable.
however, when the motor profiler option is enable, either the profiling or the normal operation are not working. It is stuck in START state.
It is stuck in START state.
I_Q_Ref is as expected but I_Q_measured is 0
Current measurement Ia and Ib are strictly identical.
R3_1_RLDetectionModeEnable is called (I am guessing by the SCC even when I try to execute normal operation) but R3_1_RLDetectionModeDisable is not called after.
Note: even the open loop voltage mode is not working anymore.
It works once for initial profiling of the motor. However I can't repeat the operation even with a new project.
I don't know what can be change in MC motorbench which can impact the motor profiler SCC.
[EXPECTED BEHAVIOR]:
Project should work either if the option of motor profiler is enable or disable
Thank you.