Profile of the trapezoidal move - position control using FOC
Can someone help me understand the profile of the trapezoidal move? for example if I would like to make a movement of 10 radiance in 10 seconds using the MC_ProgramPositionCommandMotor1 how much of the 10 seconds will be acceleration, constant velocity and deceleration? and can this profile be changed? Ideally i would like to achieve 1/6 accelleration 4/6 constant velocity and 1/6 deceleration, is this even possible? is there somewhere in the code where I can specify this?