Skip to main content
Associate II
September 4, 2025
Question

Project Generation on MC Workbench in MC_SDK v6.4.1

  • September 4, 2025
  • 1 reply
  • 379 views

Hi Team,
I have design for the custom inverter for the STM32G4A1VET6 controller and motor driver is Infineon.
custom board is designed and the while generating the code getting error as "1.4.0psdc: PSDC Version is not supported"

VINODC_0-1756994300481.jpeg

while I tried to download this package manually couldn't download showing error "FP-SNS-STBOX1" support package.

1 reply

Senior III
September 4, 2025

According to me if the project .c files are generated successfully then you can neglect the warnings.