Associate II
October 4, 2024
Solved
Remap PWM Pins
- October 4, 2024
- 1 reply
- 651 views
Hello,
I am using MCSDK_v6.3.1 and encountered a problem when changing TIM1 PWM pins:
- I cloned B-G431B-ESC1 Devkit Inverter.
- I changed High Side TIM1 PWM pins
- UH: PA8 -> PC2
- VH: PA9 -> PC1
- WH: PA10 -> PC0
When I now want to create a project with the modified inverter, I get this error:
Error
It is not possible to create a motor control project with the FOC algorithm using the selected hardware. No proper path for motor control signals was found for the following mandatory features:
- Phase Voltage Generation
For more details, please, look at the following log file in your home directory: .st_workbench/connectAlgo.log
I opened connectAlgo.log, but do not see an error.
Is this a bug?
Thanks