Skip to main content
Associate III
March 6, 2025
Solved

SDK6.3.2 completed with error

  • March 6, 2025
  • 3 replies
  • 800 views

 

Hi, Partner,

Here's the problem I've encountered and how to solve it,

I'm working with the following setup:

System: win 10 22H2, RAM 4G, i3-6100 

Hardware: Nucleo F072 + STEVAL - IPM03B +SPMSM 0.8HP + Hall sensor

Software: SDK6.3.2, Cube Max 6.13, Cube IDE 1.17

 

walen_0-1741232130261.png

Version info:
MC Workbench: 6.3.2
WB_to_Mx : 6.2.3. template-24-04-17
STM32CubeMX: 6.13.0
MC Firmware Library: 6.3.2-Full

Generation options:
Target Toolchain : ST STM32CubeIDE
Target Driver : LL - Low Level
Target STM32 FW : Latest

walen_0-1741233581851.png

walen_1-1741233729764.png

 

 

Best answer by GMA

Hello @walen,

Does STM32Cube_FW_F0_V1.11.5 at least, installed on your CubeMx tool as mentioned on MCSDK6.3.2 Release Note?

3 replies

GMA
Technical Moderator
March 6, 2025

Hello @walen,

As for your previous post, as generation ends with main.c file, can you proceed with the generated project?

You can update errors_to_skip[] struct (errors will be skipped and no more displayed) and erros_to_war[] struct (errors will be displayed as warnings in orange, preferable solution), in wb2mx.properties file located in "MC_SDK_xxx\Utilities\PC_Software\STMCWB\config".

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA
walenAuthor
Associate III
March 6, 2025

1. Can't ,when opening the project in STcube IDE and building it, there are six errors.

 

2. Great, thank you. Why does "Updater is busy" happen? SDK 6.3.2 works fine now—what might be causing issues with SDK 5.4.8?

GMA
GMABest answer
Technical Moderator
March 6, 2025

Hello @walen,

Does STM32Cube_FW_F0_V1.11.5 at least, installed on your CubeMx tool as mentioned on MCSDK6.3.2 Release Note?

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA
walenAuthor
Associate III
March 7, 2025

Dear GMA,

What is stopping it from working?

C:\Users\walen_chang.ALATECHTW\STM32Cube\Repository\STM32Cube_FW_F0_V1.11.5

walen_0-1741319545181.png