Question
Second NTC_Handle_t type sensor
uC = STSPIN32G4
second sensor = PA4 (ADC2_IN17)
I have tried add second NTC sensor and using MC functions.
A have added:
sConfig.Channel = ADC_CHANNEL_17; // BEARING_TEMPERATURE
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_47CYCLES_5;
sConfig.SingleDiff = ADC_SINGLE_ENDED;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK)
{
Error_Handler();
}to MX_ADC2_Init.
I defined :
NTC_Handle_t Temp2Sensor_M1 =
{
.bSensorType = REAL_SENSOR,
.TempRegConv =
{
.regADC = ADC2,
.channel = MC_ADC_CHANNEL_17,
.samplingTime = M1_TEMP_SAMPLING_TIME,
},
.hLowPassFilterBW = M1_TEMP_SW_FILTER_BW_FACTOR,
.hOverTempThreshold = (uint16_t)(OV_TEMPERATURE_THRESHOLD_d),
.hOverTempDeactThreshold = (uint16_t)(OV_TEMPERATURE_THRESHOLD_d - OV_TEMPERATURE_HYSTERESIS_d),
.hSensitivity = (uint16_t)(ADC_REFERENCE_VOLTAGE/dV_dT),
.wV0 = (uint16_t)(V0_V *65536/ ADC_REFERENCE_VOLTAGE),
.hT0 = T0_C,
};and in main :
NTC_Init(&Temp2Sensor_M1);Nothing happens... Do You know what I can do next?
Even is it posiible to use diffrerent /anotherADC to RCM_RegisterRegConv() function?
Kind regards
�?ukasz �?ęcki