Skip to main content
Associate III
August 26, 2025
Solved

Set hall sensor parameters with the result from ST Motor Profiler?

  • August 26, 2025
  • 1 reply
  • 701 views

Hello Everybody,

Here are the software and boards in this case:

1. MC workbench 6.3.2
2. NUCLEO-F401RE
3. X-NUCLEO-IHM08M1

I try to use the boards to obtain motor parameters. Now I got the result as illustrated in the picture? Should I set the parameter "placement electrical angle" to 131? Thank you!

small_MT_hall_param_good.jpg

Best answer by STuser2

If you check the MCSDK documentation of the hall sensor profiling example

STuser2_0-1756202928197.png

you will get the placement angle on the top they are calculating as 360 + (-56-67/2).  

STuser2_1-1756203076658.png

In your case the profiling is not complete i think it is not 100% and you did not get the value.

1 reply

STuser2Best answer
Senior III
August 26, 2025

If you check the MCSDK documentation of the hall sensor profiling example

STuser2_0-1756202928197.png

you will get the placement angle on the top they are calculating as 360 + (-56-67/2).  

STuser2_1-1756203076658.png

In your case the profiling is not complete i think it is not 100% and you did not get the value.

DF_MCAuthor
Associate III
August 29, 2025

Hello, thanks for your reply. So in my case, I should calculate the placement angle with (68+57)/2=62, right? Thanks a lot.

XY_MOTO_Hall_parameter_good_up.jpg