SPI encoder implementation.
Hi
I am looking for hints - how to implement the encoder from which I read the position via SPI?
Should I set the encoder with index in Motor Control Workbench? If so, where to write the position read after SPI to "pretend" an ordinary encoder? I also see that the encoder index (Z) raises an exception - this is where the motor speed is taken? Generally I want to use the motor in position mode with torque control.
Have any of you already run the SPI encoder with MCW?