ST Motor Control Workbench Stuck at project generation
Hi there!
I am trying to spin a motor with a STM32F3 MCU and the Motor Control SDK.
I am able to use the Motor Profiler to generate a profile of my PMSM and spin the motor via the computer. Importing the motor profile into the ST Motor Control Workbench also works fine.
When I try to generate the project files in the ST Motor Control Workbench, no files are generated and the window seems to be stuck forever without any log output in the project file generation window or in the main window.
My Setup:
HW:
- NUCLEO-F302R8 Logic Board
- X-NUCLEO-IHM07M1 Power Stage
- MAXON ECi PMSM Motor
SW:
- STM32CubeIDE 1.4.0
- STM32CubeMX 6.4.0
- Motor Profiler 5.Y.3
- Motor Control Workbench 5.Y.3
- "Firmware Package Version" was installed via CubeMX, is found by Motor Control Workbench and is available in: STM32FW V1.11.2 and STM32FW V1.11.3
Computer HW/SW:
- Tried on two machines with WIN10, both show the same result.
My Steps so far:
- Assemble HW (stack the two boards, attach Motor (maxon ECi))
- Connect Nucleo Board to PC
- Connect to Board via motor profiler
- Update FW on Nucleo Board via motor profiler (probably had some other stuff on it...)
- Run Profiling and save
- New Project in ST Motor Control Workbench with motor profile
- Check Pinout - ok
- Generate Code via dialog. Tried all Versions of the Firmware Package Version and both HAL and LL options.
- The Window "Project Generation" then stays open forever and does not show any log output or files.
Any Ideas how we can get this to run? Any Input is highly appreciated!
Thanks and stay safe!
Jakob