Startup failure at load
I profiled my motor using the Profiler application while it was not under load. Afterward, I used the obtained values to generate new software. However, during testing on the motor pilot application, the motor does not start under load, regardless of whether it’s in torque mode or speed mode. When it’s not under load, there are no issues. Do I need to perform PID tuning?
here are videos under load and not load https://youtu.be/hOYXae-8l-M?si=RV6EAJ2st8wsGWhU
https://youtu.be/sTGa2zcNCKY?si=5_LyxKUZ59Qp4z13 • The Profiler application cannot obtain values when the motor is under load.