STEVAL-CTM012V1 Not Supported in MCSDK v6.3.0, stmcx and JSON File from Website Not Compatible
- May 13, 2025
- 1 reply
- 645 views
Hello ST Community,
I'm currently working with the STEVAL-CTM012V1 evaluation board and have encountered an issue using it with the latest Motor Control SDK (MCSDK) v6.3.0.
This board does not appear in the supported hardware list of MCSDK v6.3.0, so I downloaded the firmware package for it from the official ST product page. The package is based on MCSDK v5.4.4, and the PDF with that instructs me to load the configuration file named “STEVAL-M01xV11shunt_FOC.stmcx” using the Motor Control Workbench. The .stmcx file is not detected or listed when I try to import it in MC Workbench v6.3.0 and the provided inverter JSON file (STEVAL-CTM01xV1.json) shows as invalid when I try to import it via the Board Manager, Screenshot attached. As a result, I’m unable to open or upgrade the project for use in the latest SDK.
Could you please advise:
Is there an updated configuration package (JSON and STMCX) for MCSDK v6.3.0?
If not, what is the correct procedure to migrate a v5.4.4 project to MCSDK v6.3.0?
Will support for the STEVAL-CTM012V1 be added in a future SDK release?
Your help would be greatly appreciated.
Best regards,
Sunil