Skip to main content
Associate II
January 30, 2024
Solved

STEVAL-CTM01xV1 firmware

  • January 30, 2024
  • 2 replies
  • 1910 views

Hi.
I have the IDE with the STEVAL-CTM01xV1 shunt_FOC and downloaded on the Board. As the example came, the motor doesen't work.

I opened the main.c file and I could see that it does not have any function inside the main while(1) loop. How could I have a working example to start testing the board?

This topic has been closed for replies.
Best answer by GMA

Hello,

Readme.txt is automatically opened once you select the example, I have attached the file in my previous response.

Selecting the monitor mode, you can select the motors and start/stop buttons.

GMA_0-1706770658327.png

 

2 replies

GMA
Technical Moderator
January 31, 2024

Hello,

Did you go through readme.txt document?
As mentioned in the readme.txt, for testing "6. Run the example : through the STM32 MC Workbench monitor GUI (Start Motor), or/and by pressing the Start/Stop button."
This example is for a Selni motor.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA
PGinhsonAuthor
Associate II
January 31, 2024

Thank you, but...

Where is the start/stop button on STEVAL-CTM011V1?

GMA
GMABest answer
Technical Moderator
February 1, 2024

Hello,

Readme.txt is automatically opened once you select the example, I have attached the file in my previous response.

Selecting the monitor mode, you can select the motors and start/stop buttons.

GMA_0-1706770658327.png

 

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA