Skip to main content
Associate
January 6, 2026
Question

STEVAL-ESC001V1

  • January 6, 2026
  • 1 reply
  • 306 views

I am working with the following tool versions:

  • MC Workbench: v5.4.8
  • STM32 Firmware Package: v1.11.3
  • STM32CubeMX: v5.6.1

Since I don’t have the Bull Running C1700KV motor, I’m using a 900KV motor with a 6S battery. I’ve already run the profiler, obtained the motor results, and entered those parameters into MCSDK.

My question is: Which additional parameters should I adjust to generate reliable firmware for this setup?

 

1 reply

Senior III
January 7, 2026

What do you mean by additional parameters? The latest version of MCSDK is 6.4.

aj8791Author
Associate
January 8, 2026

MCSDK 6.4 is not working for STEVAL-ESC001V1

GMA
Technical Moderator
January 8, 2026

Hello @aj8791,

STEVAL-ESC001V1 and Bull Running C1700KV motor use case operates in 6-step mode with MCSDK version 6.4.1.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA