Visitor II
June 5, 2022
Question
STEVAL-SPIN3201 ST Motor Control Workbench 5.Y.4 Generation failed
- June 5, 2022
- 1 reply
- 841 views
Attempting to load the STEVAL-SPIN3201 example from MCWorkbench 5.Y.4 and attempting to generate the code for the board doesn't work. Attempting to build the resulting project from STM32CubeIDE doesn't work. So I'm guessing that's because the generation didn't work. I'm wondering if the SPIN3201 is at it's EOL? And should I go with some other hardware instead? Or is this problem fixable?