STEVAL-SPIN3202 Correct positions of the jumpers
Dear ST,
Could you please advice on the correct positions of STEVAL-SPIN3202 jumpers to run an example with ST MotorPilot.
J9 - BOOT0 Open or closed?
J7 - RX - TX Open or closed, Could you please explain why would we need to connect RX and TX?
Which of the following ports is correct for use in ST MotorPilot? Seems that COM3?
Where can I download a bin file to test hardware for this board.
Regards,
Edward.