STM32G0B1KB and STSPIN220 motor control for custom PCB
Hi, I am a total noob at designing custom PCBs and I could use a bit of help.
My application is that I want to move a stepper motor to roughly 10 preset positions. I am using a STM32G0B1KB in my design because I need the USB and USB-PD support for my application, but I also see that that the STM32G0B1 supports some motor control functions.
From browsing online I have found that the STM32G0 does not support position control. If I were to connect it to the STSPIN220 would I then be able to navigate to the preset coordinates? If it cannot, is there a different microcontroller with 30-48 pins that supports USB data, USB power delivery, and stepper motor position control?
My stepper motor runs at 5.4V.