Question
STSPIN32F0: Why does BLDC Motor stop with a Speed Feedback Fault on Loading it?
Hello All,
I am using STSPIN32F0 controller to run a BLDC motor at 1400 RPM. I am using ST Motor Control Workbench and IAR IDE for my project.
Motor Design Specs:
Rated Voltage: 36V
Rated Current: 10Amp
Rated RPM: 1400 RPM
- My Motor Starts without any issues
- Till the Motor is loaded up to 2 Amps, it works perfectly well
- If More than 2 Amp is loaded, the Motor fails to RUN and a SPEED FEEDBACK ERROR or OVER VOLTAGE ERROR is generated.
What can be the problem?
Need your support as soon as possible.
Thank you
Ritul Shah