STSPIN32G4 Driver Output Anomaly
I designed my own PCB based on the EVSTSPIN32G4 evaluation board and created a project in STM32Cube IDE. When testing the STSPIN32G4’s internal driver, I encountered an issue: no matter what I do, the GHS voltage remains at 5.8V, the GLS voltage is 0V, and the OUT voltage is also 5.8V. I have tried setting PE8 to high or ground, as well as using PWM, but the voltage on GHS1 never rises. Reading the I²C register values does not trigger any protection; the STBY value is 0 and does not enter low-power mode; the nFAULT pin remains low regardless. As far as I can tell, there are no errors. Could an expert please provide some guidance? Thank you.
The ST Community moderator has translated the post to comply with the language of the Community which is English. For more information, see: ST Community Terms and Conditions - STMicroelectronics Community
Translated with DeepL.com (free version)