Skip to main content
Associate II
November 27, 2023
Question

Switching between Position Control and Speed/Torque Control in MC SDK

  • November 27, 2023
  • 1 reply
  • 3220 views

I have a MC Workbench generated project for the NUCLEO-401 that's working great, running in position control mode.  Is it possible to switch in realtime between position control and torque/speed control?  I'd like to home my motor by applying a known torque into a pair of stops, but then switch to position control once I've established the "home positions" of my motor.  It looks like the speed/torque control component is sort of a subcomponent of the position control and this might be straightforward, but I thought I'd ask for the canonical solution before I go hacking on it myself.

1 reply

Associate III
February 29, 2024

Hi @rsturmer-410 ,
I am trying to do something similar on an EVSPIN but the firmware is the same as yours.
Were you able to switch between the two modes in the same project/firmware?
Best

smaiti

Associate II
April 4, 2024

Yes, I did eventually figure this out.  There are API calls to enable/disable the position control, and you can call the speed controller directly when the position controller is out of the loop.  If you still need more detail on this, let me know and I can give more specifics.

 

Associate III
April 4, 2024

Hi @rsturmer-410 ,

I would appreciate it if you could share some examples to use the APIs you mentioned.
Regards
Soutrik