Skip to main content
Associate II
November 8, 2023
Question

synchronize ADC at the middle of the up-down counter

  • November 8, 2023
  • 3 replies
  • 1783 views

Hi

How to synchronize ADC triggering at the peak of the up-down counter ?

ADC1 is triggered using TIM1 trigger out event, and TIM1 has center counter mode as aligned mode3. 

Thank you in advance !

This topic has been closed for replies.

3 replies

ST Employee
November 8, 2023

Hello @VidhiPa

Configure the TIM1 trigger event as an Update event and counter mode as center-aligned mode 3 

Configure the ADC external trigger source as TIM1 trigger out event. 

Also, could you specify which board are you using? 

Thank you!

VidhiPaAuthor
Associate II
November 8, 2023

Hi Sarra, 

Thank you for replying, that is what I have done and I have the trigger event but at the start of the ARR value, I would like to have the trigger at ARR, which would be the midpoint of up down counter as shown in the below image. 

VidhiPa_0-1699454081061.png

 

I am working with STM32G431. 

ST Employee
November 8, 2023

oh, I see, thank you for the explanation,

Taking into account that you are using center-aligned mode, which alalternates between counting up (0 -> ARR) and counting down (ARR-> 0) to make a period, once the counter reaches the ARR, you trig the ADC. To do that you should interconnect the TRGO signal of your timer to the ADCx that you want to use for conversion using EXTSEL in the ADC_CFGR register.

VidhiPaAuthor
Associate II
November 8, 2023

I have settings as below:

with the settings of ADC trigger as below, I have connected TIM1 to ADC1 using TRGO2.

hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIG_T1_TRGO2;

But now the question is how do i set the TIM1 in a way that can give me trigger as explained in above post. I have 3 channels of TIM1 generating 3 PWMs. Channel 4, 5 and 6 are not being used. 

VidhiPaAuthor
Associate II
November 8, 2023

I am not using ADC in injected mode  but in scan conversion mode.