Skip to main content
yang2
Associate III
September 20, 2024
Question

The question of Timer break configuration

  • September 20, 2024
  • 1 reply
  • 513 views

Dear All,

I am currently configuring the break function of TIM1 on the STM32H5. Does anyone know the difference between these two polarity settings?

(I am unable to distinguish between these two settings. If I set one to high and the other to low, is the actual fault signal active low or high?)

yang2_0-1726798353184.png

 

    1 reply

    GMA
    Technical Moderator
    September 20, 2024

    Hello @yang2,

    Please refer to RM0481 document, "Break and Break2 circuitry overview" figure:

    GMA_0-1726820597847.png

    You can let BKxP to High (as default setting) and BKxINP will gives the needed polarity.

    If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA