Skip to main content
Associate
October 31, 2023
Solved

There is no NUCLEO-STM32F103RB board in SDK 6.0. How can I add this board on SDK 6?

  • October 31, 2023
  • 4 replies
  • 1963 views

Osman_Faruk_Avc_0-1698787759564.pngPicture 1 SDK 6

Osman_Faruk_Avc_1-1698788186795.pngpicture 2 SDK 5.4.8

 

Hello,
I want to drive a BLDC motor via IHM16M1 with the newly purchased nucleo-stm32f103rb board. But the control cart is not here. Old version SDKs are also available as XML files(f103rb). SDK 6 introduced the .json extension. And it can't generate code in older SDK versions.

Can anyone help me drive the motor?

 

    This topic has been closed for replies.
    Best answer by Gael A

    Hello Osman_Faruk_Avcı,

    Unfortunately, the STM32F103 MCU is no longer supported by our MCSDK. If you want to work on the NUCLEO-F103RB board, you need to use MCSDK version 5.4.8 which is the last version supporting F1 MCUs.

    4 replies

    AScha.3
    Super User
    October 31, 2023

    what stm32f103 card ?

    "If you feel a post has answered your question, please click ""Accept as Solution""."
    Associate
    October 31, 2023

    Stm32f103rb board

    AScha.3
    Super User
    October 31, 2023

     nucleo or what ?

    show pic...name of cpu is not enough.

    "If you feel a post has answered your question, please click ""Accept as Solution""."
    Associate
    October 31, 2023

    Yes nucleo. 

    4B3FC83E-D188-4D13-B360-4EC2F0EBE99B.jpeg

    Gael A
    Gael ABest answer
    ST Employee
    November 2, 2023

    Hello Osman_Faruk_Avcı,

    Unfortunately, the STM32F103 MCU is no longer supported by our MCSDK. If you want to work on the NUCLEO-F103RB board, you need to use MCSDK version 5.4.8 which is the last version supporting F1 MCUs.

    If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.Hope this will help,Gaël A.