Skip to main content
Associate II
August 1, 2025
Question

Torque control - speed feedback error

  • August 1, 2025
  • 1 reply
  • 204 views

Dear Support team,

I am currently working on a NucleoF302R8 and IHM07M1 driver to run a 24V PMSM motor (rated at 3600 RPM, no load).

I'm using STM32 Motor Control Workbench version 6.4.0. Whenever I attempt torque control, I consistently encounter a speed feedback failure. I've tried lowering the C2 Leuenberger constant, but the issue persists. Interestingly, this problem doesn't occur in speed control mode—everything functions correctly when running in speed control.

I would appreciate your assistance in understanding and resolving this issue.

1 reply

GMA
Technical Moderator
August 5, 2025

Hello @Abhishek_n17,

By default, the workbench tool does not set an Iq Torque target:

GMA_0-1754409183290.png

You can set a default target during the project generation step or in the MC Pilot user interface before starting the motor:

GMA_1-1754409331406.png

 

 

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA