Skip to main content
Associate III
October 24, 2023
Solved

Unable to generate ioc file

  • October 24, 2023
  • 1 reply
  • 1879 views

[VERSION]: MCSDK 6.2.0,STM32CubeMX 6.9.2
[TOOL]: MotorControl Workbench 6.2.0
[DETAILS]: I want to add my custom control board,but it say "Unable to generate ioc file due to: The following has evaluated to null or missing".
My custom control board is STM32F405RGT6, but my attempt failed. Then I try STM32F401RDTx, it is same.

1.create mcu json (STM32F401RDTx), copy from STM32F401RETx.json.

I have to add an MCU that is not in the list, otherwise my custom control board will not be displayed correctly.

微信截图_20231024154149.png   Then in this STM32F401RDTx.json file, I replace "STM32F401RETx"  with "STM32F401RDTx" , and change the flash size to "flash" : 384.  The two are just different in flash size, I think it works fine.

2.Create new board using Board Manager.  Clone from NUCLEO-F401RE.

微信截图_20231024155733.png

Then change the mcu name.

微信截图_20231024160205.png

3.Create new project

微信截图_20231024160438.png

STM32F401RD+IHM17M1

微信截图_20231024160558.png

Then generate the project.

微信截图_20231024160728.png

 

I want to know how to solve this problem.

This topic has been closed for replies.
Best answer by cedric H

Hello @gtop.1 ,

Thank you for your post.

Allowing the users to custom their boards is limited to the boards. The production of the mcu definitions from the user is not something we support. In the 6.2.0 release, we did a huge effort to support all the parts number of few series : STM32F0, STM32F3, STM32G0, STM32G4, STM32H5, STM32C0. Unfortunately, it is not the case yet for STM32F4. It is why the json definitions of STM32F4 are still limited to few MCUs.

In your case, as it is just a matter of flash size. I strongly advise you to stay with the supported MCU, it will not hurt the binary generation and download into the target.

Regards

Cedric

1 reply

cedric H
cedric HBest answer
Technical Moderator
October 24, 2023

Hello @gtop.1 ,

Thank you for your post.

Allowing the users to custom their boards is limited to the boards. The production of the mcu definitions from the user is not something we support. In the 6.2.0 release, we did a huge effort to support all the parts number of few series : STM32F0, STM32F3, STM32G0, STM32G4, STM32H5, STM32C0. Unfortunately, it is not the case yet for STM32F4. It is why the json definitions of STM32F4 are still limited to few MCUs.

In your case, as it is just a matter of flash size. I strongly advise you to stay with the supported MCU, it will not hurt the binary generation and download into the target.

Regards

Cedric

gtop.1Author
Associate III
October 26, 2023

I‘m so sad. Then I will use STM32F407 first.