Skip to main content
Visitor II
August 15, 2024
Question

UNABLE TO LOAD CUSTOM REGISTER FILE-MOTOR PILOT-MCSDK V6.3.0

  • August 15, 2024
  • 0 replies
  • 468 views

I have made some custom register json file which i want to load in my motor pilot but when i go into the motor pilot i dont get the option to load the json file:
1. I tried and overwrite and json file which gets loaded by default and i can see my registers in motor pilot BUT there are some registers which i want to write value at which im not able to do.

attached is the screenshot

motor_profiler_issue.PNG