Unable to start motor with MC sdk generated code
hi,
I have been trying to run PMSM motors with B-G431B-ESC1, I follow the steps given in the user manual,
1. I profile the motor and save the parameters
2. use the motor control workbench to generate a project, and generate source code,
3. run it in Cube IDE to flash it on the development board.
However, I am unable to run my motor with that source code. The motor doesn't even start. I also face inconsistency when running the motor with the same source code on different occasions. What could be the issue, and what should I do to resolve this issue?
since the profiler is working, where can I get a profiler code based on which the profiling .hex file is created to debug the issue?
Thank you,
Madhav