using stm32wl55ccu to drive 3 phase bldc
Hi ,
I am using stm32wl55ccu 48 pin QFN MCU to drive a 3 phase brushless motor using 3-phase complementary PWM output signals using TIMER 1. I have seen at the datasheet that this 48 QFN package is missing the complementary output of TIMER1 ,Channel 3, TIM1_CH3N (which is present at the BGA version). Is it possible to generate the 3-rd phase complementary output PWM signal in another way ?(like using timer 2 in a master/slave configuration).
Thank you, Joe.