Skip to main content
aPott.1
Visitor II
August 5, 2022
Question

What is the time scale in plot of ST Motor pilot?

  • August 5, 2022
  • 1 reply
  • 624 views

0693W00000QN2upQAD.pngHi everyone! I use ST Motor pilot to control the motor. The motor reference is 354 RPM. Quantity of pole pairs is 10. Phase period must be 60 / (354 * 10) = 17 ms. But when I display the electrical phase plot, I see that the period of the phase is 136 units. What do these units mean? ms or us?

This topic has been closed for replies.

1 reply

GMA
Technical Moderator
August 11, 2022

Hello,

Samples rate is (PWM Periode)*(execution rate). E.g for a PWM frequency 20kHz and Execution rate 2, sample are at a rate of 100us/units.

Best regards.

GMA

If you agree with the answer, please accept it by clicking on 'Accept as solution'.Best regards.GMA