Where does G431 TIM1 ITR1 acturlly from?
Hello everyone!
I use a BLDC with hall sensors drivered by ST's B-G431B-ESC1 inverter board, and demo code generated by MC Workbench.
Use ST Motor pilot V1.2.5 - MC_FOC_SDK have a test, BLDC is runing and everything is ok.
In the demo code, TIM4 use OC2REF trgo, and TIM1 is set in Trigger Mode and Trigger Source is ITR1. I have checked STM32G4 series User Reference Manual which named RM0440 from v.7 to v.8, it is show that TIM1's trigger source ITR1 is internal connected to tim2_trgo. Wow, I'm confused!
Once i modified the demo code from <TIM1.InputTrigger = TIM_TS_ITR1 > to <TIM1.InputTrigger = TIM_TS_ITR3 > as RM0440 described, PC software ST Motor pilot V1.2.5 - MC_FOC_SDK can not connect inverter board, so that BLDC can not run.
I really need your help.Thank you so much!
photos down are demo code configuration.