Skip to main content
GFrid.2
Associate II
October 5, 2021
Question

Where to find STM32F401RE .ioc file compatible with X-CUBE-SPN15?

  • October 5, 2021
  • 2 replies
  • 1045 views

Hello,

I purchased X-NUCLEO-IHM15A1 DC Brush motor controller, which is supported by BSP X-CUBE-SPN15. Documentation specifies three supported Nucleo-64 boards; I purchased NUCLEO-STM32F401RE.

How to find the F401RE .ioc file to enable resources needed by IHM15A1?

Thank you.

This topic has been closed for replies.

2 replies

GFrid.2
GFrid.2Author
Associate II
October 12, 2021

Apparently the SPN15 software was developed before MX .ioc files where created? Thus no .ioc file?

IHM15A1 mostly works, but still have not determined why Motor B will not run backward with the demo software in DUAL mode. Have replaced both the F401RE MCU and the IHM15A1Motor Driver board. Have also swapped the motors between Channel A & Channel B. The IHM15A!/SPN15 software does not drive Motor B during demo steps 1-4 with the hardware jumper set to DUAL. It all works fine in PARALLEL,

It seems likely that there may be a defect with the particular IHM15A1 expansion boards that I purchased, because it looks like the SPN15 software works just fine.

Mat1
Associate III
November 29, 2022

An *.ioc file for the X-NUCLEO-IHM15A1 would be very helpful.

Now I have to transfer the old SPN15 world to the new *.ioc world. I will use the X-NUCLEO-IHM15A1 together with the NUCLEO-F091RC.