Question
Why MCU in STEVAL-CTM010V1 example (F303VBT) on Motor C.W. SDK do not match with MCU Schematics. (F303RBT)?
The example "STEVAL-CTM010V1 dual drive with PFC" will run OK generating code correctly in SDK version 5.4.8, but the MCU inside are the STM32F303VBTx (100pin) and the Schema & Board has differently MCU. (STM32F303RBT6 - 64 pin).
How we can recompile it? The example do not accept MCU changes and remove PFC code.
Any help are welcome!