Workbench_6.3.0 Motor Control Protocol Rx 0F 04 04 C0
Using the motor control program generated by Workbench_6.3.0, Motor Pilot_6 can communicate normally. However, when sending manually using a serial port assistant, it always replies with 0F 04 04 C0 and cannot communicate normally. This issue does not occur with the motor control program generated by Workbench_6.2.1.
[16:15:36.452]TX→◇85 FF FF BF
[16:15:36.460]RX←◆05 C3 00 D4
[16:15:41.357]TX→◇05 C3 00 D4
[16:15:41.369]RX←◆05 C3 00 D4
[16:15:48.537]TX→◇06 00 00 60
[16:15:48.543]RX←◆F6 00 00 C0
[16:15:59.895]TX→◇49 00 00 70 10 00 28 00
[16:16:01.375]TX→◇49 00 00 70 10 00 28 00
[16:16:01.380]RX←◆0F 04 04 C0 0F 04 04 C0